Advanced Compact Loaders: Increase Your Workload Capacity with a Limited Fleet

by New member SkidSteerJeff ‎06-07-2016 02:16 PM - edited ‎06-07-2016 02:21 PM

blog-border-image.jpgToday’s advanced compact loaders are helping contractors further increase their workload capacity by performing a diverse set of tasks in an efficient manner. From innovations in equipment design to advancements in machine operating software, there is a range of options available to enable you to bid on the jobs you want and get the most out of your machine.

               

Utilize Attachments to Tackle Numerous Tasks with One Machine

A common concern throughout the industry is having the capacity to complete a variety of tasks with a limited number of machines. With the right attachments, a single piece of equipment can carry out tasks that would normally require multiple machines. Today’s advanced attachments can help you carry out all phases of a construction project, from site prep to clean-up.

 

Application

Relevant Attachments 

                                Capabilities

Site Prep

 

Brushcutter

Mulcher

Grapple bucket

Grapple rake

Stump grinder

 

Mowing, mulching, moving material and grinding stumps

Flatwork and      

Foundation

 

Bucket

Hammer

Pallet fork

Blade

Drum compactor

 

Smoothing dirt, spreading gravel and transporting palletized cinder block

Structure and

Utilities 

 

Bucket

Pallet fork

Trencher

Backhoe

 

Moving structural materials, trenching, digging for underground utilities

Landscape

 

 

Pallet fork

Auger

Power box rake

Landscape rake

Landscape tiller

 

Leveling dirt, removing rock, setting sod, planting trees

Clean-Up 

 

Angle broom

Utility broom

Bucket

Grapple bucket

Sweeping and collecting debris, dumping scrap material

 

Performance Matching Your Machine and Attachments

Without a doubt, you are going to get the greatest productivity out of your machine and attachments when the equipment is performance matched. To performance match your equipment, it is recommended to use attachments engineered by the same manufacturer as your machine because the tools are specifically designed to fit and maximize performance on    the manufacturer’s compact loaders. 

 

Additionally, it’s a good idea to consider features that are designed to increase efficiency and ease-of-use for the operator. For example:

 

  • Return-to-dig and work tool positioners allow operators to pre-set the attachment angle and automatically recall that setting when requested. This helps create easier loading cycles, reduce cycle times, and judge proper depth and back drag angles.
  • Electronic dual self-leveling helps keep the attachment level and prevents it from tilting forward when lowering the lift arms. Without this feature, operators would have to manually adjust the work tool angle each time they lower the lift arms and attachment.
  • Creep mode gives operators the ability to adjust ground speed independent of engine speed. Traveling at a slow ground speed with full engine horsepower and hydraulic flow is especially useful for rotary tool applications such as trenching and brush cutting. 
  • A high hydraulic flow and high pressure option comes in handy when you are working with attachments that require both speed and torque to maximize performance and production, such as mulchers and cold planers.
  • Electronic couplers allow operators to change out attachments using controls from within the cab and in a shorter amount of time than with manual couplers.

 

Advancements in Machine Control Pattern Options

Since different operators have different control pattern preferences, it’s good to know that some manufacturers offer more than one control pattern option for their compact machines. Today’s control pattern options include:

 

  • ISO pattern controls which employ one hand drive and one hand operation of the implements.
  • H-pattern controls which employ two hand drive and two hand operation of the implements.
  • Hand and Foot Controls which employ two hand drive and two foot operation of the implements.

 

Advanced control features let you customize the controls to your preference, allowing you to tailor the drive and implement response to your experience level or task. Additionally, advancements in joystick controls inside the cab are also helping to improve operator comfort and reduce fatigue. 

 

Cab Design that Increases Operator Comfort and Safety

               

Operators are often exposed to potentially harmful particles in the air on the jobsite. Fully sealed and pressurized cabs can help minimize inhalation of particles and dust that mix in with the air during everyday operations. Sealed cabs are also quieter, which allows operators to focus on the tasks at hand and reduces their fatigue at the end of a long day.

 

These cabs are also designed to improve visibility. Rearview cameras with in-cab display are now being installed in newer model compact loaders—allowing operators to be fully aware of their 360-degree surroundings without having to turn their head.

 

To learn more about extending your workload capacity and the features available on today’s advanced compact loaders that help you do so, contact your local Cat® dealer or visit us online.

 

We’d like to hear about how you are increasing your workload capacity and project efficiency.  

  • Tell us about your fleet. Do you operate compact loaders? Track or wheeled machines?
  • Do you utilize attachments to increase workload capacity?
  • Which attachments do you utilize most often? On which types of applications?
  • Do you purchase all of your attachments? Do you ever rent attachments?
  • Do you stick to “one brand” for your machines and attachments or do you “mix and match?”
  • Are there certain machine features or advancements that are helping you extend your workload capacity and efficiency? Which ones?
  • Are there features, advancements or attachments you wish you had to help increase your capacity or get the job done faster?

Comments
by IBRAHIM Najem
on ‎07-11-2016 03:21 PM
I looking for
Cat 950 f from 1997 to 2000

Thanks
by Contributor idigcat
on ‎07-11-2016 04:13 PM

IBRAHIM Najem,

 

If you are located in the United States or Canada, you can visit our Cat Used website:

www.catused.com.

 

If you are located outside of North America, we recommend contacting your local Cat Dealer: http://www.cat.com/en_US/support/dealer-locator.html

 

Thank you for your interest in Cat machines.

by Jayesh Jani
on ‎09-26-2016 01:31 AM

Great Blog !

Thank you for sharing this post.

About the Author
  • I am a Pre-Field Agriculture/Product Application Representative for Caterpillar. I recently graduated from North Carolina State University with a dual degree in Agriculture Business Management and Agriculture Science, concentrating in Leadership and Environmental Technologies. I focus primarily on the relationships between customers, dealers, and the product specialists for the Building Construction Products division. Growing up on a beef cattle farm, I have several years of machine operation experience and agricultural knowledge. Thomas Jefferson said it best in that, "Agriculture is our wisest pursuit, because it will in the end contribute most to real wealth, good morals, and happiness."
  • I’m a Compact Wheel Loader Product Application Specialist for Caterpillar in North America. I have 11 years of experience, including roles in the field as a dealer technical support representative, and as a distributor business model consultant.  I graduated from North Carolina State University with a Mechanical Engineering Degree, and wanted a job where I didn't have to sit in front of a computer all day.  This job allows me to get out and get my hands dirty, with the goal of providing solutions to customers’ machine needs.
  • I am a Marketing Communications Specialist for Caterpillar with over twelve years of experience marketing the Cat brand to customers in Latin and North America. My goal is to arm customers with the information needed to make well informed purchase decisions; to maximize the value of Cat machines by using an array of Cat Work Tool attachments; and to minimize the total cost of ownership by using Cat parts and Cat Dealer service.
  • I am an expert Operator and Application Specialist for Caterpillar concentrating on products used in the construction trades industry. I operate, evaluate and train on Cat machines and Work Tool Attachments worldwide. I have a Degree in Agricultural Engineering, Craftsman Certified and was named Apprentice of the Year 1981 at the University of East Anglia, UK.
  • I am the National Association Manager for Caterpillar and have responsibility for customer associations and partnerships in multiple industries for Caterpillar. I have 12 years of experience at Caterpillar, and have spent most of those years in the field with dealers and customers around North America. I have always had a passion for equipment and find myself fortunate to be able to work with dealers and customers almost every day.
  • I am a Product Application Specialist with 16 years of experience in the industry. As a Building Construction Products Global Trainer, I focus on training dealers and customers on machines, attachments and applications as it relates to the construction, agriculture and landscaping segments.
  • I have been with Caterpillar for more than eight years, working in various roles including a materials engineer, a filters product manager and my current position as a parts consultant. My job allows me the opportunity to work with Cat dealers and customers providing insight on how the use of quality filters and fluids results in better equipment performance and lower owning and operating costs.
  • I am a marketing and sales support professional for Caterpillar. In this role, I work with our marketing and customer service teams to support or dealers and customers, concentrating on our Small Wheel Loader, Skid Steer Loader, Mini Excavator and Dozer product groups. The exchange of ideas, information and opinions about equipment and how it’s used in various industries on forums such as this blog helps me fulfill my role at Caterpillar to the best of my ability.
  • I am the commercial/market consulting expert for all Caterpillar tires and rims with 14 years of experience. I provide guidance in the harsher work environments of mining and industrial/waste applications. Our goal is to turn our dealers and customers into knowledgeable and trusted resources with respect to tires and rims. Our group offers training, technical support and resources to develop a level of expertise within the Caterpillar value stream that is ordinarily reserved for tire companies and local tire service providers. Ultimately, we want to provide our customers with a total Cat solution from the ground up.
  • I am a Sales Support Manager for Cat Financial and have responsibility for ensuring that the right financial products are available to Cat customers who purchase, lease or rent to own. 8 of my 10 years with Caterpillar Financial have allowed customer and/or dealer interaction as part of my daily responsibilities including over 3.5 years as a Territory Manager. I take personal satisfaction in finding financial solutions that work for our customers and CAT dealers.
  • I’m a Telehandler Product Application Specialist for Caterpillar in North and South America. I have 13 years of experience, including roles in the field as a dealer service operations and technical support representative, and as a distributor business model consultant. My telehandler passion and focus is working with dealers and customers to maximize the versatility of the product through machine and operator training.
  • I am a Product and Application Specialist with over 35 years experience at Caterpillar. I focus on helping you to determine the best Cat machines, work tool attachments, and services for you to use in the building and general construction, landscaping, specialty trades, and agricultural industries.
  • I am a Senior Regional Insurance Marketing Manager with 16 years’ experience at Caterpillar Financial Insurance Services. I have the opportunity to work with 18 North American dealers providing risk management products and services that helps the Caterpillar Enterprise ( Caterpillar, Dealers and Customers) manage their business risk. Caterpillar Financial Insurance Services offers Extended Protection Plans for machines and engines, Physical Damage Insurance, Inventory Protection Plans, Dealer Property and Casualty, Risk Management, Marine Transit Insurance and Dealer Bonds.
  • Jeff Brown is a marketing professional for Caterpillar Skid Steer, Multi Terrain and Compact Track Loaders. Over Jeff's 12 years in the industry, he has visited with and studied the needs of customers across landscaping, construction, and agriculture segments. Delivering innovative solutions that solve customer's problems is Jeff's main focus.
  • I am a North American Product and Application Specialist for Caterpillar. In this role, I have had the opportunity to represent Caterpillar at various trade shows and train customers on new Small Wheel Loader content. I graduated from Purdue University in 2001 with a Mechanical Engineering degree and have spent the past 15 years with Caterpillar in various engineering roles. Growing up in the Mid-West, I have always loved the cold and the unique activities winter enables. Unfortunately, I had to give those up when I moved to North Carolina. I don't care what people say, you never get used to a hot climate.
  • I am a Filter and Fluid Marketing Consultant with over 14 years experience working at Caterpillar. My focus is to ensure customers understand the importance of using superior filtration and lubrication products in their equipment.
  • I am a Sales Support Manager with over nine years of experience in a variety of roles with Caterpillar Financial Services Corporation. Throughout my career, I have had the opportunity to gain experience in matching financial products and tailoring funding strategies to the specific needs of customers. This includes more than three years as a Territory Manager in Seattle partnered with N C Machinery, an authorized Cat dealer covering the states of Washington and Alaska.
Announcements

Welcome to the Construction Trades Online Community!

This online discussion forum is for construction and landscape professionals to raise issues, voice opinions, gain insight and share knowledge so we can all build on each other's expertise.

First Time Users: View Guidelines and Tips in the Welcome Board
Questions and Comments: Post in the Feedback & Suggestions Board
Help Us Grow the Caterpillar Community: Invite a Friend

Labels