Going Above and Beyond Tier 4 Final Standards for Rental Power Applications

by New member riderdw on ‎10-17-2016 08:00 AM

Darryl Rider Blog.jpg

 

Since 2008, the Environmental Protection Agency (EPA) has been phasing in a series of “tiered” emission regulations to reduce harmful exhaust gas for diesel powered equipment.  The standards require significant emission reductions of particulate matter (PM) and nitrogen oxides (NOx).

 

Today’s Tier 4 Final emission standards represent a 95% reduction in emission levels compared to non-regulated amounts. As government mandates, all new products must meet these requirements, but machine owners can still elect to use existing equipment.  

 

Therefore, the responsibility solely falls on engine manufacturers to not only meet these requirements but do so while maintaining qualities that are advantageous to the rental power industry such as performance, reliability, productivity and cost.

 

PM is defined as the black smoke or soot found in diesel engine exhaust, and NOx is defined as nitrogen monoxide and nitrogen dioxide. Tier 4 standards require that both be significantly reduced; however the two work independently and against each other. There are technologies that lower PM, but often increase the NOx levels and vice versa.

 

As a result, engine manufacturers implement various strategies to meet stringent Tier 4 standards while also bringing enough added value to encourage rental operations to actively select these solutions.  

 

In-cylinder advancements

Tier 4 solutions often offer advanced fuel injection systems, which precisely control the fueling process through a series of carefully timed microbursts. This injection timing provides greater control of combustion for the cleanest, most efficient fuel burn. In a rental setting, generator sets are often utilized in remote or unattended locations. But increased fuel efficiency can result in less frequent refueling charges, which saves the customers costs over the rental period.

 

Exhaust gas recirculation (EGR) may also be utilized to lower the engine’s combustion temperature. The EGR valve allows a small amount of non-combustible exhaust gas to re-enter the engine cylinder and combine with the combustion air. This lowers the combustion temperature and reduces the level of NOx output. By optimizing combustion, fuel consumption is lowered thus reducing the amount of diesel exhaust fluid (DEF) required.

 

Aftertreatment technology

Beyond in-cylinder advancements, a variety of aftertreatment components are available to complement engine optimization to exceed customer expectations for productivity, fuel efficiency and service life.  In this process, gases flow through the canister and are brought in contact with the catalyst that oxidizes the unburned hydrocarbons (HC) to reduce emissions.

 

A diesel particulate filter (DPF) is a device designed to capture diesel particulate matter or soot from the exhaust stream of a diesel engine. The device uses a series of alternately block channels within the filter to force exhaust gas to flow through the walls and capture PM.

 

Selective catalytic reduction (SCR) is a technology that injects a small amount of DEF into the exhaust upstream of a catalytic chamber. An electronic controlled DEF injector sprays a precise amount of DEF into the exhaust stream. Most engines have a targeted flow rate of 2-3% of diesel fuel consumed. When the DEF and exhaust enter the catalytic chamber, a chemical reaction occurs that converts NOx to nitrogen (N2) and water (H2O). In a rental application, SCR allows for lower fuel consumption through combustion optimization and increased productivity.

 

Regeneration

As previously established, Tier 4 Final solutions require that PM or soot must be removed from the DPF to ensure emissions criteria are achieved. The process is called regeneration and there are two available options for engine manufacturers.  

 

The first method of regeneration is passive regeneration. In a passive regeneration system, the DPF restores on its own during normal operation. Most passive regeneration systems introduce an oxidation catalyst into the process to oxidize the PM, but to create the oxidation the exhaust temperature must be raised. Because of this, passive regeneration is not preferred by rental applications, as many operations are lightly loaded and do not reach the optimum temperature for regeneration to occur. Some manufacturers that rely on passive regeneration have incorporated an on-board load bank to increase the load in order to meet the required exhaust temperature for regeneration to occur. This adds increased cost and components to the generator set.

 

A more efficient regeneration method for rental applications is active regeneration. In an active regeneration system, the soot level of the DPF is monitored and it triggers regeneration when thresholds are reached. When the system requires regeneration, it will induce it and utilize a fuel burner that will burn or oxidize the soot over the catalyst. This strategy will be more efficient in rental applications, where load levels may fluctuate. Regeneration will occur independently of the load variation and ensure optimal performance of the DPF.

 

Fluid Specifications

A built-in fuel efficiency benefit of Tier 4 Final solutions is the required use of ultra-low sulfur diesel fuel (ULSD). The improved fuel blend reduces the sulfur content from 500 ppm in low sulfur diesel fuel to 15 ppm in ULSD.  Although ULSD fuel comes at a higher cost, this will be somewhat offset by the increased fuel efficiency of up to 5%. Improved fuel efficiency can translate to thousands of dollars over a given rental period. Plus, using fuels with higher levels of sulfur often results in operational problems and jeopardizes component life. ULSD can be utilized in all legacy engines as well, so there is no need to purchase multiple fuels.

 

_________________________________________________________________________________

 

With today’s Tier 4 Final standards, engine manufacturers are going above and beyond to strategically and systematically implement technologies that not only meet stringent requirements but also establish these solutions as beneficial assets to any rental operation.

 

We want to hear from you.

 

  • How are you impacted by Tier 4 Final emission standards?
  • Have you experienced any long term benefits from selecting a Tier 4 Final solution?
  • Does improved fuel efficiency play a role in selecting a solution?

 

Comments
by Susan Lara
on ‎10-19-2016 09:35 AM

Very informative article. The technologies discussed are a need of the hour. We can save big on electricity at our home, we can use presently expencive renewable energy but at the same time we should make the non-renewable technologies far more effecient than before. These non-renewable still covers the major part of electricity/energy production. Across the world the developing nations and the new emerging markets like China nad India can benefit a lot with these new efficient technolies. They are also a major contributor to carbon emmission and with these Tier 4 level standards they can control that. 

by Essay writers uk
on ‎01-10-2017 02:42 AM

The  Environmental Protection Agency (EPA) ia facing a serious issue and the blog post discuss about the solutions to overcome it. I think the four technologies In-cylinder advancements,Aftertreatment technology,Regeneration,are the best solution to overcome it.

by Buy research proposal
on ‎01-10-2017 04:37 AM

EPA has taken some decisions and they follow some strategies to reduce harmful exhaust gas. In this blod, we can see the details of the emission level and the percentage of reduction. 

by New member teamouting
on ‎01-23-2017 05:05 AM

Environmental Protection Agency is a great one. we all should protect our enviornment properly. these should be for the next generation too. so we should kept it in a good mannaer. in my city im working in a team outing bangalore company. here all the people care these things. 

by Mitchell Starc
on ‎04-01-2017 01:44 AM

Beyond Tier 4 Final Standards for Rental Power Applications, it is really an innovation in saving expenses on fuel. Ultra-low sulphur diesel fuel is authentic for all kinds of the engine. Good contribution.In reality, I am a writer at Quality Custom CV Editing Service.  I am also doing my side work in power rental house that's why this blog is very illuminating for me.

by academic assignment writing
on ‎04-28-2017 02:18 AM

The Environmental Protection Agency (EPA) I am facing a serious issue and the blog post discuss about the solutions to overcome it. I think the four technologies In-cylinder advancements, Aftertreatment technology, Regeneration are the best solution to overcome it.

by Programming Homework Help
on ‎05-26-2017 11:21 PM

Hi buddy, your blog' s design is simple and clean and i like it. Programming Homework Help
 Your blog posts about Online writing Help are superb. Please keep them coming. Greets!

by Buy R Programming Assignment
on ‎05-27-2017 12:02 AM

Great Information,it has lot for stuff which is informative.I will share the post with my friends.

by Solidworks Project Help
on ‎05-27-2017 12:20 AM

The leading assignment help UK firm offers state of the art services to its clients with a promise of delivering all the required work well within the deadline.

by Digital Marketing Agency
on ‎05-27-2017 12:47 AM

This is really a great stuff for sharing. Thanks for sharing.

by 任务帮助
on ‎05-27-2017 01:04 AM

好的帖子,这将是伟大的所有人,非常感谢传播这个信息在这里。

by Take My Online Exam For Me
on ‎05-27-2017 01:17 AM

I appreciate this work amazing post for us I like it.

Announcements
Help us grow the Caterpillar Community: Invite a Friend

Meet Our Bloggers