Reply
New member

3196 intermittent issue with accelerating past 1500 rpm - Turbo sensors ??

Greetings, 

I've just joined the forum in the hope of receiving some comments and suggestions about an intermittent issue I am experiencing on my boat. 

The vessel seems to get stuck / wont accelerate past 1500 rpm, it feels like the turbo's just arent kicking in and then the engines are limited to this speed.

 

Boat is a 2000 48 Riviera fitted with twin 3196 660hp Caterpillars, engine have had scheduled services their entire life and most recently less than 20 hrs ago, clean hull, 1/4 tank in fuel and otherwise all is normal load. 

 

Top speed previously was 28 knots at around 2,200 rpm, now cant do more than 1500rpm and just 14 knots.

There is no smoke, 

Air cleaners have been replaced 

Fuel filters replaced

Injectors cleaned

Port engine Turbo has been removed cleaned and rebuilt, 

Port engine aftercooler was removed and cleaned. 

 

The issue was originally identified by the Cat technician as being the Sensors for the Turbo Part #169-3725 which they replaced with new model part #218-3840.

 

After replacing the sensors the vessel pushed past 1500rpm and reached max 2100rpm without issue, upon our next cruise though the issue returned. 

 

Removing, cleaning and or changing sensors seems have a result and the boat performs well however the issue is intermittant and then returns. We've tried swapping sensors from other boats and also from the Fuel system Part #161-9930 however the problem is still not 100% resolved. 

 

Please any idea, suggestions very much welcomed.