Reply
New member

3208 gauge installation Help

[ Edited ]

HI 
I bought a 1988 motor yacht witch has twin 3208TA 375hp in it. all the gauges are not installed and the old ones are (before I bought the boat) cutted away. I have three gauges that I need to install and i will put the pictures of them down below. 

where is the sensores on motor that go to the gauges? 19349233_10209235769440368_354137929_o.jpg