Reply
New member

Engine crankcase pressure

en la serie C32 serial RXB de 1800hp EUI cual es el rango de operacion de la contrapresion del carter. existe una tabla con dichos valores gracias 

New member

Re: C32 is smoking and has high crankcase pressure.

What is the serial number of the C32? if its sxc......, there is PIP on the Liner, Piston, ring and the sump of this ( SXC......) then one or two piston may likely got broken. just remove the oil sump for metal filing. you better stop runing the engine to avoid futher damage

Cat Dealer
Dealer

Re: C32 is smoking and has high crankcase pressure.

[ Edited ]

This sounds very much like an injector issue. There will be no alarms if the problem is mechanical so this will need to be checked out. A few simple tests using ET would quickly diagnose a specific cylinder and pinpoint the problem.

New member

C32 is smoking and has high crankcase pressure.

My
2008 c32 started smoking and thumping noise was comming out exhaust. Had high crank case pressure. Changed Ccv filter thinking that was cause of problem but still smokes at start up and the noise is the same. I have had no alarms..