Reply
Highlighted
Contributor

Re: INJECTOR SOLENOID TEST NOT OK ( *OPEN )

thanks GHarms09

now my problem solved, i found the pin connector at ECM got problem,....the pin connector has been repaired,..

 

thanks friend,...

Regular Contributor

Re: INJECTOR SOLENOID TEST NOT OK ( *OPEN )

Usually an "Open" Is an wire/pin unplugged or solenoid failed. Always verify the pins are all pushed into the connectors properly at every connection and at the ECM. Do the CAT 5lbs pull test on the wires as well in case the wires have come loose from the pins.

If you have a spare ECM around from same model it wouldn't hurt to try. If you have a blank ECM use the "TEST ECM" mode to try it.

Another way to check is make 2 jumpers to run to neighboring injectors and do the solenoid test. If test fails the same injector number then you know it's not an injector problem but a wiring issue or possible ECM issues. Easy test to do before buying an injector.
Contributor
Accepted Solution

INJECTOR SOLENOID TEST NOT OK ( *OPEN )

dear all,

 

i have CAT marin engine 9KS01720, my problem is injector solenoid test no 5 recorded not OK (*open), so what kind of the problem?...anyone can explain me pls,

 

note:

1. the injector already change

2. the resistance and continuity of the cable was ok

 

is my ECM got problem?