Reply
Super Contributor

Re: Shutdown?

Remove the shut-down solenoid from the governor and look inside the governor at the shut-down linkage. I've seen the screws for the small paddle loosen up and the shut-down solenoid will not properly actuate the linkage. The governor will need to be disassembled to repair if that's the case.
Contributor

Re: Shutdown?

Problem continues ?

Motor will continue to run for 20 / 30 min. At idle then will shut down. Cannot feel any type of click at pump. When I depress stop all gauges go to 0 motor continues to run. Tempature is at 180. I cleaned all contacts. .

Contributor

Re: Shutdown?

Thank you Will check

Bob

Super Contributor

Re: Shutdown?

I assume this is an ETS system (energize to stop). If the stop solenoid does not click when depressing the stop button, I'd check the relay first.
Contributor

Shutdown?

Have 3126 cat with 700 hrs. That will not shut down. 1999 mfg. year.

I can turn off key battery and all electrics, still runs. After 30 40 min. Will turn key back on press stop and unit will stop ? Does not happen on all trips appreciate any leads thank you!