Reply
Highlighted
Contributor

Re: TEMPORARY RUN ENGINE WITHOUT A WORKING TURBO

Thanks so much! really appreciate the info.

Super Contributor

Re: TEMPORARY RUN ENGINE WITHOUT A WORKING TURBO

Actually, you can pre-lube the turbo and then just start engine normally and let idle for a few minutes.
Contributor

Re: TEMPORARY RUN ENGINE WITHOUT A WORKING TURBO

Thanks for the resonse and advise. Got a replacement cartridge, I understand the procedure is to first oil prime the turbo, spin the fan, then tumble the engine with the stop button pressed for 10-15 seconds, then start and let idle for about 10 minutes before testing at high RPMs. is this correct and is there anything else I should know.

Super Contributor

Re: TEMPORARY RUN ENGINE WITHOUT A WORKING TURBO

Don't even try to start it.
Contributor
Accepted Solution

TEMPORARY RUN ENGINE WITHOUT A WORKING TURBO

My 3126B engine's turbo broke. That is to say the shaft that holds the two fans snapped. The dealer here in Trinidad does not have a new cartridge on hand. My question is can I put the cartridge minus the fans and shaft back into the turbo housing and use the engine at low rpm for the weekend. Will the oil go directly into my aftercooler and clog it or is there a possibility of my engine running away.  or do I just run the boat on one engine for now. the serial is 3GS00302 and this is a 455 HP 3126B marine engine.