Reply
Trusted Contributor
Trusted Contributor

Re: G3616/3612 LE A4 Engines

Also, remember that the connection is not what determines the exhaust back pressure.  You have to determine if the 18 inch pipe at whatever length you will be using will accommodate the engineexhaust flow volume without exceeding the back pressure limit.  It might be that the G3616 A4 exhaust pipe size might have to be larger (including the catalyst) to keep from exceeding the limit.  With this in mind, it is easy to see how Cat has decided to use one exhaust outlet size.

 

Best Regards,

Al Hunt

New member

Re: 3606 LE A3 differences from 3606 LE A4 Engine

Thank you for checking.

Trusted Contributor
Trusted Contributor

Re: G3616/3612 LE A4 Engines

The technical information for the G3600 A4 states that the maximum exhaust back pressure is 12 inches of water for all four engine models.  While I haven't looked into the numbers and calculated the differences, I would say that Cat has determined that the 18 inch exhaust size will not cause the maximum back pressure to be exceeded. 

 

When Cat states this maximum back pressure, this is not a shutdown value but it will impact the fuel economy, maybe the emissions and the exhaust temperature.  Many times with the G360 A3, the additional restriction caused by adding an oxidation catalyst increases the normal back pressure near the A3 back pressure limit.  So I don't see anything by using the same size exhaust for both the G3612 A4 and the G3616 A4.

 

Best Regards,

Al Hunt

New member

Re: G3616/3612 LE A4 Engines

I'm surprised to see the same size engine outlet given the large difference in exhaust flow rate between the G3616 / G3612. 

 

 

Caterpillar Style 2 Flange Dimensions via Belmar Industries 

 

SizeStyle NoIDODBCDHole SizeNo of HolesTHKWt
18218.121.8520.870.54160.526

 

Typical Exhaust Flow Conditions: 

G3616 A4 

  • 30,697 acfm
  • 840 °F

G3612 A4

  • 23,315 acfm
  • 824 °F

Estimated Engine Outlet Velocity:

 

G3616 A4 with 18" CAT Flange

  • 286.33 - 289.52 ft/s

G3612 A4 with 18" CAT Flange

  • 217.46 - 219.90 ft/s
Trusted Contributor
Trusted Contributor

Re: 3606 LE A3 differences from 3606 LE A4 Engine

The information states that the G3612 A4 and G3616 A4 both are sized for 18 inch exhaust.  The attaching flange bolt cirle is 20.87 inch diameter; showing 0.54 inch bolt hole size,16 holes.  So this would be a common 18 inch industry exhaust connection to accommodate commonly available adapter flanges.

 

Best Regards,

Al Hunt

New member

Re: 3606 LE A3 differences from 3606 LE A4 Engine

This thread has been very helpful. I've been looking to confirm that the 3600 series engines with the ADEM4 rating have (1) inlet connection per turbo, and (1) outlet connection per engine. Based on Al's initial response it appears that this is so.

 

I also want to confirm the exhaust connection's flange size for both the 3612 / 3616 ADEM4 rated engines since they have been updated from dual exhaust outlet to single exhaust outlet.

 

Thanks,

George Snitz

Highlighted
Trusted Contributor
Trusted Contributor

Re: 3606 LE A3 differences from 3606 LE A4 Engine

You will find information about the G3600 A4 at this link

http://www.cat.com/en_US/products/new/power-systems/oil-and-gas/gas-compression-engines/1000000844.h...

 

Best Regards,

Al Hunt

New member

Re: 3606 LE A3 differences from 3606 LE A4 Engine

Thank you very much again, your kind assistance is greatly appreciated

 

Respectfully,

Charles Sharp

Trusted Contributor
Trusted Contributor

Re: 3606 LE A3 differences from 3606 LE A4 Engine

 

Here are the spec sheet numbers for the G3600 A4:

G3606 A4         LEHW0234

G3608 A4         LEHW0235

G3612 A4         LEHW0236

G3616 A4         LEHW0198

 

Best Regards,

Al Hunt

New member

Re: 3606 LE A3 differences from 3606 LE A4 Engine

Al,

Thank you for the fast and thorough detailings on the differences, do you know if the spec sheets are available for the A4 models yet, I cannot locate them on the server.

 

Rexpectfully,

Charles Sharp