Reply
Highlighted
Contributor
Employee

HANDY HINT - WHAT IS MAX GRADIENT

Max Gradient displays the value of the maximum gradient between two points (interim point or waypoint) within a road.  

 

EXAMPLE:  If a road has 1 interim point (assume equal lengths of road between waypoints and interim point) and the road has an actual gradient of 5% but was flat between one waypoint and the interim point  Between the other waypoint and the interim point this road has an actual gradient of 10%,  the max gradient of the road would be 10%.  

 

Enjoy!! 

Kerrie