Reply
Highlighted
Contributor

Re: 3512 Stop light continues flashing

CHECK THE BATTERY CHARGING VOLTAGE IF IT GOES ABOVE 27 OR 28 VOLT CHECK THE BLCK PRESSURE SENSOR LF INSTALLED CORRECT AT 45 DEGREE ANGLE

New member

Re: 3512 Stop light continues flashing

Here include the power based instructions.continues light flashing based informations are included in this article.as i am working in the electrical services.i know more about the power instructions.if you looking more about me please visit our site Electrical Services Dubai

Super Contributor

Re: 3512 Stop light continues flashing

Possibly a parameter in the monitoring system is programmed incorrectly for the operating conditions. Look for an event code such as high altitude derate, exhaust temperature, etc.
New member

Re: 3512 Stop light continues flashing

SN:LLA02656 on Engine.
Super Contributor

Re: 3512 Stop light continues flashing

What is the genset serial number?
New member

3512 Stop light continues flashing

When engine is put to auto after 20 seconds the engine stop light starts flashing. When started, at idle and at run it continues. The generator can be put on line and on load with the light still flashing. There are no fault codes in the diagnostics and it can not be cleared by pressing the alarm silence button. Thank you for any replies.