Reply
Highlighted
New member

Re: Engine 3508B, Serial number 7SM00195

Thank you friend. I replace the 4 sensors. I also bought the sensor connections to the motor. I'm in Tallinn, EST and will be now going to TURKU, FIN. I'll have the Caterpillar technician travel with the ship to do a machine test. After replacing the sensors and using the CAT ET DATA LINK, no further error was displayed on the computer.
Super Contributor

Re: Engine 3508B, Serial number 7SM00195

There 2 speed-timing sensors on the left rear of the engine. If the primary fails, the engine will continue to run on the secondary sensor. Both sensors are the same part number.
New member
Accepted Solution

Engine 3508B, Serial number 7SM00195

Hello. I'm the Chief Engineer of the "CISNE BRANCO" Ship-Sailing Machines. My engine has a problem with intermittent shutdowns. So far we have not been able to resolve. I wonder if anyone has ever had a similar problem. I suspect either the magnetic pick-up sensor, short-circuit or low insulation. Could someone help me with this?