Reply
New member

3406C fire pump engine

Hello. We recently installed a new stationary 3406C fire pump engine, which meets the NFPA-20 standards. It can start both manual or automatically from fire pump controller panel; however, it cannot be stopped either from controller pump panel or from engine panel. Only can be stopped actuating the stop lever on the injection pump.  What can be wrong with the electric stopping of this engine?

Super Contributor

Re: 3406C fire pump engine

Sounds like the engine shut-off wiring could be incorrect. Most fire pump engine shut down systems are ETS (energize to shut off). The controls need to energize the shutdown solenoid thru a timer (usually 8 seconds or so).
New member PPS
New member

Re: 3406C fire pump engine

Dave, sorry to barge in on this thread, but would you have the approximate weight of a D399 Block Bare?

Getting ready to move one out of an engine room and need some idea before I do the rigging.

 

Thanks

Highlighted
Super Contributor

Re: 3406C fire pump engine

Bare block is a little over 4000 lbs.