Reply
Visitor

Remote Start Connection for a model 3406 engine with EMCP II

I have a year 2002 model 3406 engine with SR4B generator and I want to connect a remote start.  The drawing shows wire 30 and 57 as as my connections however I can't find 57 any body have an idea were it is?

Super Contributor

Re: Remote Start Connection for a model 3406 engine with EMCP II

A handfull of different designs in those days, in reality, the IC contact is across battery negative and the START input from the ECS to the EMCP II, just take a look at your print and you'll be able to figure out where the customer connection is.

 

Mike L.

Cat Dealer
Dealer

Re: Remote Start Connection for a model 3406 engine with EMCP II

Mabry,

 

According to drawing, wire 30 and 57 are used as Remote Start signal.

Wire 30 is conected to battery negative(-). Wire 2 is also conected to battery negative. it is easy to find the wire.

WIre 57 is connected to Chassis Customer Terminal 12, connected to Door terminal 7 , to GSC port 33 through 40 way harness conector linked to GSC.

You can find the wire from GSC, then to terminal.

 

Regards,

 

wc2008

New member

Re: Remote Start Connection for a model 3406 engine with EMCP II

Tell me pls which  pins to connect for auto start mode in EMCP2 CONTROL PANEL for 3406 cat genset , yom is 1999

Regards