Reply
Highlighted
New member

Allowable Transient loading of 1360KVA DG- Model-3512B

Dear Sir,

 

For our Doha South STP project, we have puchased New CAT DG's. Details of Alternator/ Engine/ CT ratio/ Breaker at DG alternator end are enclosed herewith, kindly clarify us what is the maximum transient current/ load can be applied for more than 30 sec.

 

Alternatively, we would like to connect a load of 500KW (blower motor) using a soft stater (Schnieder - ATS48M12Q) with the pre- set value of 350% limiting current for 20Sec accelaration ramp time with the starting torque of .

 

Please note we succesfuly carried out load test at 110%.