Reply
New member

Re: G3520C Fuel Correction Factor

 
Visitor ZR
Visitor

Re: G3520C Fuel Correction Factor

The fuel correction factor will be different due to the condition of each engine. One engine could have more wear than the other. Excessive wear on the turbo charger, blowby, etc. Our 3520s are never at the same fuel correction level. 8.2% O2 seems very high compared to our sites. Typical we run below 2% and have ran up to 5%. The higher the O2 the more probabilty of taking out turbos and cyliner heads upon hard shutdowns. Witnessed this on other makes also. There should be no issue using a 4-20 as long as it is scaled. Although the engins will run a lower methane number they dont quit like it. So depending on your site it will depend. Tailor it to your site but within specs.  You might want 4 at 40% and 20 at 65% really depends on the characteristics at your site.

Contributor

G3520C Fuel Correction Factor

Hello.

 

We have 6 engines at a LFG in argentina.

 

We seted the window for the signal of CH4 level in that way:

 

           LLHV       HLHV         Use Fuel Quality
          MJ/Nm3  MJ/Nm3           MJ/Nm3           Fuel Correction Factor
GE 1 12,5          26,4                  20,36               104
GE 2 12             26,8              20,08                    106
GE 3 12              27,2                 20,79               102
GE 4 12,5            26,8                20,4                100
GE 5 12             27,2              20,24                    100
GE 6 13,7          26,5            20,64                      100

CH4 Level informed by FSU Landtec 57,1%

 

this values were found with a O2 around 8.2% and NOx around 140 ppm.

 

we have 2 questions
- Why the difference in the FCF (Fuel Correction Factor), in some cases the FCF for the engine 2 is 112 and at the same moment for the engine 6 is 100.
- Is ok that we send a signal 4..20 mA with the level of methane or it need a conversion to other value.

regards