Reply
New member

Looking for a copy of D2 Testing for 3 engines

Hi-

 

I am looking at trying to get ahold of copies of the original EPA D2 testing for the following 3 engine models:

 

2004   4CPXL78.1ERK    Model:3516B         2847.5 HP

2005   5CPXL78.1ERK    Model:3516B         2847.5 HP

2010   ACPXL105.T2E    Model:C175-16      4423    HP

 

I am really interested in the exhaust Gas Flow (CFM), Exhaust Gas Temperature (F)

of each load level.

 

Typical load levels: 10%, 25%, 50%, 75%, 100%.

 

I would love any and all data related to the testing!

 

If anyone has copies, please let me have a copy!

 

Thanks!