Reply
Highlighted
New member

Re: 3512B-DI-SWAC Main Propulsion Fault codes

Thanks Dave10010,

 

I replaced the ECM and injector #12. During our next passage we had another set of codes appear on the same engine, which I was hoping someone could help me with. 

 

030 248 F02

030 819 F02

033 012 F05

 

I dont have CAT ET with me onboard right now but I suspect another bad injector??

 

Thanks in advance.

 

 

Super Contributor

Re: 3512B-DI-SWAC Main Propulsion Fault codes

All those faults suggest a failing engine ECM. 030-819 F02 is a data link fault to the electronic display. 033-254 F12 is an ECM fault and the other is an injector fault. Injector faults often happen when the ECM is failing. Your engine has a back-up ECM so you should not be dead in the water but you should get this problem repaired by your local Cat dealer ASAP.
New member

3512B-DI-SWAC Main Propulsion Fault codes

Hi all,

 

Was hoping someone could help me identify some fault codes on our CAT 3512B main propulsion engine. The Engine model # is 3512B-DI-SWAC and Serial # is 7HM00164. The Engines are a bit older and the codes displayed on the EDM are:-

 

030 819 F02

033 254 F12 SERV CODE

033 007 F05 SERV CODE 

 

Thanks in advance!