Reply
Super Contributor

Re: Communication Adaptor 3 windows 10 problem

Powering the comm adapter thru the PC can cause communication problems so it's not recommended. Latest firmware is 1.23.54. Use the comm adapter tool kit in the ET utilities menu.
Visitor

Re: Communication Adaptor 3 windows 10 problem

also comm adapter can be powered from the pc. when ı used  comm adapter with windows 8 power led is on(ı connect the comm adapter just pc),. but with windows10 it is not powered.

 

ı think an new firmware required for windows10.

 

 

Super Contributor

Re: Communication Adaptor 3 windows 10 problem

The comm adapter should not be powered from the PC. It should only be powered when connected to an engine or machine.
Visitor

Communication Adaptor 3 windows 10 problem

hi!

 

I install windows 10 to my pc. after that ı cannot use adaptor 3. ı have ET2016B.

power dont come to the adaptor form the pc. Do you know any new firmware update??