Reply
Contributor

Re: i have done lot off sea trial.

hi..

 

how much %load is appearing ont he monitoring panel at clucthin condition.? 

is it showing more than the normal case?

and the propeller is too heavy for this engine rating.

is this original installed pro.engine or replaced by C32 with old engine?


umairanwar wrote:

c32 engine can not reach on top RPM. if rated RPM is 2300 engine reach maximum 2220 or 2250. why?

can u give me a hint how i can run engine on top rated RPM. without load it will run 2350 easily.




Trusted Contributor

Re: i have done lot off sea trial.

can  be that the vessel is loaded to heavy or is wrongly balanced, or the propellers are simply too heavy.

if the vessel is already a long time in the water marine growth can also be present causing to slow the boat down.

Regular Contributor
Employee

Re: i have done lot off sea trial.

Hi Mary,

 

Please provide us with the serial number of your engine, so that we can give you the right answer.

Best regards

fanam77
Contributor

i have done lot off sea trial.

c32 engine can not reach on top RPM. if rated RPM is 2300 engine reach maximum 2220 or 2250. why?

can u give me a hint how i can run engine on top rated RPM. without load it will run 2350 easily.

mary