Reply
Highlighted
New member

3126 Maximum Fuel flow

What is the maximum fuel flow rate for a 420 HP 3126? This is not the maximum fuel consumption for the engine, I need to know the maximum fuel flow to the motor which will include the portion returned to the fuel tank. I need to know this in order to size the flow meter range from Scintex.