Reply
Highlighted
New member

Re: CAT 745 C PROBLEM WITH TRANSMISSION

Hi

I also have problems with this transmission on my 745 (3F6).

931 HRS on clock and clutch 4 is gone.Pulled transmission (Code 674-2  Transmission Intermediate Speed Sensor #1   Occ 126 times.)

Other truck on site also has the same problems.

Dealer advise is run it till destruction. Caterpillar will then perform PIP.

Big egg in Cat's face i would say. 

 

New member

CAT 745 C PROBLEM WITH TRANSMISSION

Hi all,

I have problem with CAT 745 C transmission , all cat 745C truck shows intermediate speed sensor error , when I check the sensor ,it is struck by transmission gear while this is fixed sensor, can't be adjusted, looks like too much play on transmission gear, what should I do to minimize it. as anotice I already replace transmision on one of my machine. thanks