Reply
New member

B20D Odometer Issues

Hi, I've got a B20D that's logging different engine hours on the display as opposed to what's being broadcast on the CAN bus.

 

This is the CAN bus data log in terms of the engine hours (my apologies for the formatting):

 

391 12:15:48.886 18FEE500 Rx 61 D0 05 00 FF FF FF FF
2578 12:15:53.798 18FEE500 Rx 61 D0 05 00 FF FF FF FF
4791 12:15:58.717 18FEE500 Rx 61 D0 05 00 FF FF FF FF
6985 12:16:03.640 18FEE500 Rx 61 D0 05 00 FF FF FF FF
17928 12:16:28.234 18FEE500 Rx 62 D0 05 00 FF FF FF FF
20078 12:16:33.159 18FEE500 Rx 62 D0 05 00 FF FF FF FF
22214 12:16:38.072 18FEE500 Rx 62 D0 05 00 FF FF FF FF
28730 12:16:52.842 18FEE500 Rx 62 D0 05 00 FF FF FF FF
30895 12:16:57.765 18FEE500 Rx 62 D0 05 00 FF FF FF FF
33040 12:17:02.668 18FEE500 Rx 62 D0 05 00 FF FF FF FF
37426 12:17:12.521 18FEE500 Rx 62 D0 05 00 FF FF FF FF
39631 12:17:17.433 18FEE500 Rx 62 D0 05 00 FF FF FF FF
41817 12:17:22.360 18FEE500 Rx 62 D0 05 00 FF FF FF FF
46054 12:17:32.198 18FEE500 Rx 62 D0 05 00 FF FF FF FF
48221 12:17:37.124 18FEE500 Rx 62 D0 05 00 FF FF FF FF

7762 12:18:26.095 18FEE500 Rx 62 D0 05 00 FF FF FF FF
9878 12:18:31.000 18FEE500 Rx 62 D0 05 00 FF FF FF FF
11985 12:18:35.914 18FEE500 Rx 62 D0 05 00 FF FF FF FF
14133 12:18:40.839 18FEE500 Rx 62 D0 05 00 FF FF FF FF
16234 12:18:45.748 18FEE500 Rx 62 D0 05 00 FF FF FF FF
27173 12:19:10.359 18FEE500 Rx 62 D0 05 00 FF FF FF FF
29352 12:19:15.272 18FEE500 Rx 62 D0 05 00 FF FF FF FF
33686 12:19:25.122 18FEE500 Rx 63 D0 05 00 FF FF FF FF

 

Using the FMS spec, I can see that these messages seem in the correct format and increment once every 3 minutes (as expected from the spec). This value corresponds to 19051 hrs.

 

However, on the dashboard, the value on the display reads 32626 hrs. I see no correlation between these values and I can't figure out where this value comes from, either.

 

My question is this: is this issue common on these vehicles?  Or is the display reading in different units (the ratio between the two is about 1.71)? How would I go about using these values for client feedback on engine hours?