Reply
Highlighted
New member

966G fork attachment lift point capacity

Hey folks... I am currently in Afghanistan and I need a specifications question answered. We have a fork attachment for 966G that needs to be moved to another location via helicopter. The only viable way is sling load. The attachment has two lift points welded to the top beam. Where can I find the rated capacity of these lift points??

The following numbers are on the identi plate for the attachment:

CWTS-A/AP 17

283-7988

284-7615

ARC00265

137-4234 17

 

the forks look identical to this (photo from internet):