Reply
Regular Contributor

Re: ADEM II Connections

This is also dependant on whether you are utilising the Engine start/ crank function and E stop in the ADEM ECM. If these functions are being controlled by another controller then they will need to be held low (connected to digital return)  

New member

Re: ADEM II Connections

Thanks will make sure they are jioned and give it a try 

Regular Contributor

Re: ADEM II Connections

Typo 29 - Digital Return

Regular Contributor

Re: ADEM II Connections

At the ADEM ECM P1 40 pin connector the the pins are 13 - ECS Start/Stop /Run 1 and 14 -ECS Start/Stop /Run 2 (both of these wires are joined together and should always be in the same state) , 8 - Estop 1 and 19 - E stop 2 (both of these wires are joined together and should always be in the same state) and 19 - Digital Return

Super Contributor

Re: ADEM II Connections

OK, I guess it's a non-Cat generator with neither EMCP or EMCP+. Looks like pin 8 is for remote shut-down and 29 is digital return. 13,14, and 19 are unused on gensets. Hope that helps.
New member

Re: ADEM II Connections

thats the only other name plate it had 

New member

Re: ADEM II Connections

WhatsApp Image 2018-10-19 at 8.30.13 AM.jpeg

Super Contributor

Re: ADEM II Connections

Need genset serial number, not engine serial number.
New member

Re: ADEM II Connections

WhatsApp Image 2018-10-18 at 2.40.44 PM.jpeg

Super Contributor

Re: ADEM II Connections

Post genset serial number.