Reply
Highlighted
Contributor

Re: EMCP 4.2 No Keypad Function - Root Cause

This issue is sporadic in relation to Geographic location and has been thoroughly investigated at all major manufacturing facilities that have produced this controller throughout its production life. The root cause appears to pointing fingers to hard at the EMCP. Replace the EMCP and be gentle depressing the soft keys moving forward.
Contributor

Re: EMCP 4.2 No Keypad Function - Root Cause

Good day,
I can configure new emcp4.2 via keypad without using ET.
Then what items I have to order to do this, plz waiting
Contributor

Re: EMCP 4.2 No Keypad Function - Root Cause

Sir,
Can I replace old EMCP 4.2 with a new one configurung via EMCP dispaly not by CAT ET tools. As old EMCP keypad is not working
Contributor

Re: EMCP 4.2 No Keypad Function - Root Cause

Contact to main dealer in your region
Contributor

Re: EMCP 4.2 No Keypad Function - Root Cause

I have same probelem in 7 uits, did u find any solution

Contributor

Re: EMCP 4.2 No Keypad Function - Root Cause

We had same problem in 4 of our 3512B genset, the dealer replaced it on warranty. EMCP 4.3
New member

EMCP 4.2 No Keypad Function - Root Cause

[ Edited ]

Good day!

 

Need help regarding this problem. It was confirmed that unable to navigate through the controller overview and configuration menus or non operation of the Run, Stop and Auto buttons. The customer was asking for the root cause and it was too general to say that due to internal circuitry malfunction / internal short circuit. We are not able to open the EMCP and verify the defective components because it will void the warranty. 

 

Kindly refer to media number TEBE1362-05.

 

Model: C175-16

S/N:     G2G00120 / WYB01485

 

Hoping for your positive response.

 

Best regards,

Line