Reply
New member

Re: Undervoltage problem

these companies should required some dp images and other things.

Contributor

Re: Undervoltage problem

yes,you can see fault (alarms) in CDVR soft.

PC - RS232 - com(CDVR)

Visitor

Re: Undervoltage problem

Thank you for you answer, ı changed the Cdvr, the problem was solved. But it is weird that the generator is running with bad cdvr for four hours than shut down, did you faced this situation like that? Also can ı see the cdvr failure cause by connecting with pc program?
Contributor

Re: Undervoltage problem

Emcp 2 it's not voltage regulator. Voltage regulates by CDVR (caterpillar digital volt regulator) or DVR. There are connectors check them. And try change rotating diode bridges if have spaire.
Contributor

Re: Undervoltage problem

If have CDVR check CurrentTrasformer. Socket P12 (1;2). I knew problem if it's broken, then voltage drops suddenly. Or try disconnect this pins P12(1;2) and check voltage.
Visitor

Re: Undervoltage problem

We try with load and off load, the result is same, undervoltage.emcp 2 controller we have,checked f1 and f2 cable , ok.

Do you have any opinion?
Contributor

Re: Undervoltage problem

1) is it island or parallel mode?
2) load changed or constant?
3) what controller used: EMCP, CDVR, DSE, COMAP...?
4) chech wiring: +E; -E......
More info better.
Visitor

Undervoltage problem

Hello everyone
We have a g3512 generator, the generator starting well, and working almost a hour, after that the output voltage drop suddenly, ı check permanent magnet fuses, they seems well.
İs there any suggest to solve this problem?