Reply
New member

EMCP4.2 panel + EMCP3 monitoring software?

Hi.

 

Can a EMCP4.2 panel be paired with EMCP3 monitoring software?

 

Currently I'm searching for the generator from the network and I cannot find it. 

I've tried all possible baudrates.

 

The connection goes as follows currently.:

MON PC running EMCP3 -----[COM Emulation over TCP/IP]------> MOXA 6150 ------[Serial]-----> EMCP4.2 panel..

 

Thanks in advance! 

New member

Re: EMCP4.2 panel + EMCP3 monitoring software?

Jeez, guys.

An answer would be nice.

 

Can I monitor ECMP4.2  panel through EMCP3 software? Yes/no?

New member

Re: EMCP4.2 panel + EMCP3 monitoring software?

yes .  u can monitor ! hope this works for u !

New member

Re: EMCP4.2 panel + EMCP3 monitoring software?

Yes. 
Finally got this figured out.

I had EMCP3.0 monitoring software which didn't support EMCP4.* panels.

I reached out to the guy who installed it for us and was able to get the correct software.

 

CAT should really have software on the website ready to download for generator owners.

New member

Re: EMCP4.2 panel + EMCP3 monitoring software?

You try to check back on how the baudrates look 

 

 

Tonos de llamada gratis | Sonidos de animales 

New member

Re: EMCP4.2 panel + EMCP3 monitoring software?

On the web application you can read all information from the CAT EMCP panel. You can set alarms so you get timely notification if there are situations you want to be informed about. The measurements are presented via a web application which is also available on your smartphone.

New member

Re: EMCP4.2 panel + EMCP3 monitoring software?

New member

Re: EMCP4.2 panel + EMCP3 monitoring software?

Can I monitor ECMP4.2  panel through EMCP3 software? Yes/no? Gautam Gambhir’s wife

Highlighted
New member

Re: EMCP4.2 panel + EMCP3 monitoring software?

I was thinking of non-browser apps, like PayPay, or Skype, or ebay for instance, most expensive cars in the world